Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

TI's HDC2080 Digital Humidity and Temperature Sensor, Now at Mouser, Boasts High Accuracy at Low Power for Smart Devices

 

August 16, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the HDC2080 humidity and temperature digital sensor from Texas Instruments (TI). Offering high accuracy and low power consumption in a compact package, the HDC2080 sensor is suitable for a broad range of Internet of Things (IoT) and environment-monitoring applications.

The TI HDC2080 humidity and temperature digital sensor, available from Mouser Electronics, is a capacitive-based device that uses an integrated heating element to dissipate moisture and condensation. The sensor integrates multiple digital features, allowing for the use of programmable input thresholds to deliver system wake-ups and alerts without needing to rely on a microcontroller to monitor the system. The HDC2080 sensor's low power consumption allows developers to place their microcontrollers in deep sleep mode, because the sensor can initiate measurements without input from a microcontroller. The high-performance sensors offer a typical humidity accuracy of ±2 percent and a typical temperature accuracy of ±0.2 degrees C.

The sensor features an auto measurement mode to initiate humidity and temperature measurements, enabling efficient performance in applications with power-budget restrictions. The sensor is designed for battery-operated systems and supports a supply voltage range of 1.62 V to 3.6 V. With an operating temperature range of minus 40 to 85 C, the sensors can be safely used in applications such as home appliances, smart home devices, smart thermostats, HVAC systems and inkjet printers.

The HDC2080 humidity and temperature digital sensor is supported by the HDC2080EVM, a simple plug-and-play platform that features an MSP430F5528 microcontroller and a USB interface, allowing for easy communication between the HDC2080 sensor and a PC. The module's included software graphically logs humidity and temperature data, and the module also allows access to the sensor's configuration registers.

To learn more, visit www.mouser.com/ti-hdc2080-digital-sensor.


With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room