Samtec High-Speed Cable Assemblies Now Available from Mouser
March 17, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, offers a variety of high-speed cable assemblies from Samtec.
Samtec high-speed cable assemblies include ACCELERATE® slim body, ERCD 0.80mm Edge Rate®, HLCD high-speed hermaphroditic, HQCD 0.50mm Q Strip®, and SEAC SEARAY™ series.
The ACCELERATE cable assembly consists of the ARC6 slim cable body that mates together with the ARF6 series for a secure connection.
The ERCD 0.80mm Edge Rate assemblies use Samtec's Eye Speed cable to provide a 14Gbps performance and feature a double-row system to 120 pins and a standard metal latching system. Eye Speed cable technology offers excellent signal integrity performance with individual copper serve or braid shielding, 26AWG to 38AWG coax and twinax construction, and 20Ω, 50Ω, 85Ω, and 100Ω ratings.
HLCD high-speed hermaphroditic cable assemblies are designed to mate with LSHM board-mounting connectors and feature Razor-Beam contacts for high reliability.
The HQCD series cable assemblies are compatible with the ATH and QSH ground-plane connectors and offer 50Ω single-ended signal routing, 38AWG coax cable, and a double-row system up to 180 pins.
Samtec SEAC SEARAY assemblies mate with SEARAY sockets and feature a 0.4A current rating, 120VAC voltage, and up to 95% operating humidity range.
To learn more, visit https://www.mouser.com/new/samtec/samtec-high-speed-cable-assemblies/.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 1,100 manufacturer brands. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com